This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootloader+Application, The problem of program entry address jump

Genius 3095 points

Part Number: TMS320F28377D

Dear team:

I divided the flash of f28377d into 16 blocks, The block plan is as follows:

I wrote the test project of bootloader and application respectively, and wrote the instruction to jump to application in bootloader, and added the control program of LED status light in application. In addition, I also configured the CMD files of the two programs. Below is the program:

1.1, Bootloader

1.2, Bootloader CMD file:

2.1, Application

2.2, Application CMD file

At present, the problem is that after power on, the program can run bootloader program normally, but can not jump to application program normally. It is speculated that there may be several reasons for this:

Reason 1: is there any problem in the preparation of jump instructions?

Reason 2: is there a problem with the configuration of the CMD file?

Reason 3: are there any other ignored places not configured?

Best regards