Hi
I need to know what is the reaction time of the sigma delta fast overcurrent detection in TMS320F2837xD Dual-Core Microcontroller.
The reaction time is related to the latency of the filter calculate with the following formula:
So if our data are:
Sinc filetr = sinc3
OSR = 16
Modulator rate = 20 MHz
Sinc Latency = 2.4 us => Is right?? Is this the reaction time for overcurrent detection?
It is possible to configure the comparator filter with this data and the data fileter unit with other oversampling rate (128)?
The microprocessor manual tell:
Higher threshold comparator events can be configured to trigger following events : CPU interrupt, CLA task, PWM trip.
It is possible to connect the comparator out to a digital IO without using a ISR or a CLA task?