This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: to drive a 3 phase, 220V motor using AC entry+PFC

Part Number: TMDSHVMTRPFCKIT

Hi,

I am reading the datasheet of the TMDSHVMTRPFCKIT.

As I seen, there are three ways to supply DC bus voltage for 3 phase inverter stage(1. DC supply/  2. AC entry / 3. AC entry+PFC) .

Is it possible to drive a 3 phase, 220V motor while using AC entry (170-250 Vac)+PFC?

I know that the proper dc bus for a 220 V motor is 300-320V and the nominal dc bus output of a boost-based PFC is 390 V (Vac_in: 170-265). Therefore, we cannot use PFC since the dc bus voltage is so high. 

Does the PFC is not a solution for such condition to reduce input harmonic currents of a drive? if NO, what's your suggestion?

Thanks