This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash question on 28035

Have a small piece o code that blinks LEDs. If I run it in RAM (through the XDS100 emulator it runs fine). If I program it in Flash, the following happens:

- during power up, RESET (XSR) is asserted periodically for about 8 seconds

- after the 8 seconds, the code starts running, but it runs at a much lower speed (about 2.2 times slower)

- I should mention that I did the exact same experiment using the control card for Picollo, and there is no difference in speed when running off of it.

 

Has anyone experienced such issue? Is there a fix for it?