Part Number: LAUNCHXL-F28379D
Dear All,
I am using Simulink to build a model to receive CAN messages. You can see diagram below. I am getting "error: expression must have struct or union type" error. Please help me. How can I solve that?
Thanks
"ykarata1_BMS_C2000_RX_deneme.c", line 67: error: expression must have struct or union type
"ykarata1_BMS_C2000_RX_deneme.c", line 68: error: expression must have struct or union type
"ykarata1_BMS_C2000_RX_deneme.c", line 70: error: expression must have struct or union type
"ykarata1_BMS_C2000_RX_deneme.c", line 71: error: expression must have struct or union type
"ykarata1_BMS_C2000_RX_deneme.c", line 73: error: expression must have struct or union type
/* S-Function (scanunpack): '<S1>/CAN Unpack' */
65 {
66 /* S-Function (scanunpack): '<S1>/CAN Unpack' */
67 if ((1 == ykarata1_BMS_C2000_RX_deneme_B.eCANReceive_o2[0].Length) &&
68 (ykarata1_BMS_C2000_RX_deneme_B.eCANReceive_o2[0].ID != INVALID_CAN_ID)
69 ) {
70 if ((4 == ykarata1_BMS_C2000_RX_deneme_B.eCANReceive_o2[0].ID) && (0U ==
71 ykarata1_BMS_C2000_RX_deneme_B.eCANReceive_o2[0].Extended) ) {
72 (void) memcpy(&ykarata1_BMS_C2000_RX_deneme_B.CANUnpack,
73 ykarata1_BMS_C2000_RX_deneme_B.eCANReceive_o2[0].Data,
74 1 * sizeof(uint8_T));
75 }
76 }
77 }