This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Missing Device F2806 in Devise list.



Sorry I put in wrong forum

Have the new Piccolo F2806x controlstick and CCS4.2 running (partley).

The Piccolo F2806 ins not in the device list when making a Target configuration.

Using Texas Instruments XDS100v1 USB Emulator

TMS3202806 is there.  Piccolo F28027 controlSTICK is there but not Piccolo F28026 controlSTICK

  • Hi Martin,

    You need CCS v4.2.1 or above. If you do have v4.2.1 already installed on your machine you need only to run the two executables , ti_c2000_f2806x_flash_setup_4.2.0.1.exe and ti_c2000support_setup_1.0.0.0.exe in the extras folder in the CCS install directory on the DVD. That should give you flash support as well as target configuration support.

    If you dont have v4.2.1 It is best to run the installation from the DVD and it will pull in all the other executables for flash and target config support.

    I hope this helps

  • Thanks for the answer. It worked.

    Had a couple of the CCS running and did not start afreash.

    Went and started with the CD and it worked find.

    Thanks