Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Per the TRM, the ethernet module supports IP fragmentation in HW. In chapter 43.5.6.8, the TRM states to set bits 13 and 14 in DMA_CH0_TX_CONTROL to enable IP fragmentation. However, these bits are listed as reserved and read-only.
Is this feature available? Assume this is documentation issue? Can IP fragmentation be enabled and work with DriverLib?
Thanks,
Eric