Other Parts Discussed in Thread: UNIFLASH
Dear Champs,
I am asking this for our customer.
The user could not use Uniflash or CCS to read the sector 8 starting from 0x88000.
See below figure.
It seems it has something to do with OTP because we found Z2_OTPSECLOCK is not same as normal.
They do not intend to use any CSM password, but they did intend to modify the boot mode pin from GPIO24/32 to Zero Boot Mode Select Pins and always boot to flash.
See below OTP registers
See Z2_OTPSECLOCK
Questions:
1) Their OTP setting is as below. Is there anything wrong?
In f28004x_codestartbranch.asm
In the .cmd file,
2) Is the weird Z2_OTPSECLOCK the reason that memory 0x88000 (sector 8) cannot read? Or is there any other cause?
Wayne Huang