Part Number: LAUNCHXL-F280049C
Hi,
I bought a brand new Launchpad Launchxl-F280049C. When I try to connect the USB to the CCS and try to load the code, I get the below error:
Error initializing emulator:
(Error -2071 @ 0x0)
Internal error: Missing or corrupt application file. Restart the application. If error persists, please report the error.
(Emulation package 8.1.0.00005)
When I do the Test connection in the ccxml file, I get the below error:
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
I am using CCS Version: 9.0.0.00018.
Thank you.
Gobind Singh