Part Number: TMS320F28379D
Tool/software: WEBENCH® Design Tools
Hi, there
I am using TMS320F28379D and XDS110 Debug Probe.
When I am not using EMIF, the debug probe is working fine, but when I try to use the EMIF, I see the Debug probe get disconnected and shows this:
"C28xx_CPU2: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.1.0.00001)
C28xx_CPU2: Trouble Halting Target CPU: (Error -1135 @ 0x8B0F) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.1.0.00001)
C28xx_CPU2: Unable to determine target status after 20 attempts
C28xx_CPU2: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.1.0.00001)
C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0x13425) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.1.0.00001)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging"
Another engineer in my company see the same issue. He have tried several debug probe (all XDS110) and all of them show the same issue.
I am working in a very quite environment. I don't believe there is noise around the circuit. So, here's my question:
1st. Since this is EMIF related, are there a specific EMIF setting (Hold time, Set up time ect.) will cause this kind of problem?
2nd. Are there a better debugger than XDS110 that will not have this issue?
Thanks
Eric