This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069: 在使用 Piccolo F2806x ISO controlCARDs 时遇到如下问题:

Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

请问:在使用 Piccolo F2806x ISO controlCARDs 时出现如下信息,是什么原因导致的?

Restarting Program Model...
Initializing target : C:\ti\guicomposer\eclipse\workspace\.metadata\.plugins\com.ti.binding.program\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Debug Probe/C28xx
Loading program: null
sun.org.mozilla.javascript.internal.WrappedException: Wrapped java.lang.NullPointerException (<Unknown source>#18) in <Unknown source> at line number 18Restart Completed.

  • Hi,

    Can you provide the full console output with the error message. From the initial message, I suspect your target configuration file is not correctly configured with the debugger and/or device in use. Can you send a snapshot of the target configuration settings in the appConfig.xml file that you are attempting to use.

    Are you trying to run an example in C2000Ware?

    Regards,

    Ozino