Other Parts Discussed in Thread: TMS320F280049, C2000WARE-DIGITALPOWER-SDK
Hi
Basically I am looking for TI microcontroller that can replace the features of Microchip dspic33ck256MP202T... but better analog comparator and high resolution PWM
1. supply voltage 3.3V
2. PWM with 150ps resiution and can able to generate upto 25MHz
3. atleast 3 ADC which sampling and conversion time less than 300ns
4. 3 inbuil analog comparator that can compare the analog input with the DAC value
5. atleast 2 or 3 DAC modules that can able to generate analog voltage with slope compensation with 87.5 V/ us and with minmum the resolution of 30mV. For example if I want to generate slope starts from 2.5V to 600mV within 1us
Could you please provide the P/N for me?