This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049: Can CLA trig DMA ?

Part Number: TMS320F280049

Tool/software: Code Composer Studio

Hello,

We have implemented the following system on our real time system with 280049 :

EPwm (fixed frequency 100 kHz) -> trig Adca Adcb Adcc

End Of conversion on Ada -> trig CLA for calculation

At end of CLA calculation, we have to update the Epwm CMPA (for changing duty cycle), actually, we reload the Epwm registers in the CLA return interrupt 

but it's not immediade (could be delayed by other interrupts, CAN, Timer, etc ...)

Is there a possibility, at the end of CLA calculation, to trig the DMA to reload EPwm immediately and without any program ?

Or is there any possibility to update the Epwm inside the CLA task ?

(Or another idea or solution will be wellcome)

Thank you by advance

Best regards,

francois