This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2811: Use of Address-Bit Multiprocessor Mode in the Serial Communication Interface

Part Number: TMS320F2811


The SPRU051D document describes the Address-Bit Multiprocessor mode where frames have an extra bit called an address bit. The address bit is set to 1 in the first frame of the block and 0 in all other frames.

Is it possible to implement this mode while using the receive and transmit FIFOs for the SCI?

  • Ashley,

    Address-bit mode (and idle-line mode) are independent of the enhanced FIFO feature.  The purpose of the FIFOs is to reduce servicing overhead.

    I hope this helps. If this answers your question, please click the green "Verified Answer" button. Thanks.

    - Ken

  • Ashley,

    It's been a while since I have heard from you last. Therefore, I am assuming that my last reply resolved your issue and I will close this thread. If this isn’t the case, please reject this resolution or reply to this thread. If this thread locks, please make a new thread describing the current status of your issue. Thank you.

    - Ken