Part Number: TMS320F28379D
Hello,
I have a question regarding the timing of the SDFM module.
In my application the SDFM module works with 10MHz SD-C clock. The SDFM module is synchronized to the zero event of the EPWM unit. This works fine.
Now I have found out, that there is delay between the zero event of the EPWM unit and the setting of the AF-Bit in the SDFM module which indicates new data available from the SDFM module. I have measured a delay between 520ns and 560ns.
Is this delay systematic?
I want to write a routine in order to check the synchronism between EPWM and SDFM during runtime, because a resynchronize of the SDFM module yields in wrong results for the first three cycles (with sinc3 filter).
Is it possible to rely on the delay time?
Best regards
Ralf