This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: TMS320F28379D ERRORSTS pin is always high

Part Number: TMS320F28379D


Hi there,

I'm using TMS320F28379D MCU for my application, when I upload the my final code, I'm getting ERRORSTS pin as a high. I can also run my code succesfully, I can debug the MCU but error LED is still blinking on the board. How can I remove the error ?

Thanks.

  • Hi,

    I would suggest to check the NMISHDFLG flag register and see if there is any flag set there. If yes then please see why that is set. It could be CPU2 WD reset flag which you can clear and that should fix the issue.

    Regards,

    Vivek Singh