Part Number: TMS320F28376S
Tool/software: TI C/C++ Compiler
Dear Sir ,
we are developing product based on 28376S and want to secure the memory from reverese enginnering (e.g. using JTAG connection)
i have follow the example blinky_with_DCSM and implemneted as part of the project
i have created asm file with the follwoing
.....
.cdecls "security.h"
.sect "dcsm_otp_z1_linkpointer"
.long Z1_LINK_POINTER
.long 0xFFFFFFFF
.long Z1_LINK_POINTER
.long 0xFFFFFFFF
.long Z1_LINK_POINTER
.long 0xFFFFFFFF
.sect "dcsm_otp_z1_pswdlock"
.long 0xFFFFFF77
.long 0xFFFFFFFF
.sect "dcsm_otp_z1_crclock"
;; .long 0xFFFFFFFF
;; .long 0xFFFFFFFF
.sect "dcsm_otp_z1_bootctrl"
;; .long 0xFFFFFFFF
;; .long 0xFFFFFFFF
.sect "dcsm_zsel_z1"
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xDFFFFFFF ;Z1-GRABRAM , CLA - Zone1,LSx and Dx are secure
.long 0xD5555555 ;Z1-GRABSECT , All allocated to Zone1
.long PASSWORD_KEY0 ;Z1-CSMPSWD0 (LSW of 128-bit password)
.long PASSWORD_KEY1 ;Z1-CSMPSWD1
.long PASSWORD_KEY2 ;Z1-CSMPSWD2
.long PASSWORD_KEY3 ;Z1-CSMPSWD3 (MSW of 128-bit password)
where PASSWORD_KEY0 ....PASSWORD_KEY3 (is key i have defined )
and Z1_LINK_POINTER is definde set to 0x1FFFFFFF e.g. Zone selct block will be located at 0x78020
in the linker command i have added
PAGE 0:
....
DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C
/* Z1 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004
/* Z1 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004
/* Z1 OTP. RESERVED/BOOTCTRL */
DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z1 OTP. Z1 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010
/* Z2 OTP. LinkPointers */
DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C
/* Z2 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004
/* Z2 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004
/* Z2 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004
/* Z2 OTP. GPREG3/BOOTCTRL */
DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z2 OTP. Z2 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010
.......
SECTIONS
{
/*OTP*/
dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0
dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0
dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0//
dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT
dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT
}
The software is combied from
a.custom bootloader - runs after reset , unsecure the DCSM if neceassry for programing flash and them resecure
b.main application
for unsecure procedure (e.g. 4xdummy read and them write 4x key)
void UnsecureMemory()
{
volatile int tmp;
int I;
unsigned long LinkPointer;
unsigned long *Zone1SelBlockPtr;
int bitpos = 28;
int ZeroFound = 0;
// volatile long *CSM = (volatile long int *) 0x5F010; //CSM register file
volatile long *CSMPWL = (volatile long int *) 0x78080; //CSM Password location (assuming
LinkPointer = DcsmZ1Regs.Z1_LINKPOINTER.all;
/*find zone select block by finding '0' MSB in Z1LINKPOINTER*/
while ((ZeroFound == 0) && (bitpos > -1))
{
if ((LinkPointer & 0x80000000) == 0)
{
ZeroFound = 1;
Zone1SelBlockPtr = (unsigned long *) (0x78000 + ((bitpos + 3) * 16));
}
else
{
bitpos--;
LinkPointer = LinkPointer << 1;
}
}
if (ZeroFound == 0)
{
Zone1SelBlockPtr = (unsigned long *)0x78020;
}
/*Password are offset by RECORED (E.G. OFFSET 0x8 from zone select block*/
CSMPWL=Zone1SelBlockPtr+4;
for (I = 0; I < 4; I++)
tmp = *CSMPWL++;
DcsmZ1Regs.Z1_CSMKEY0 = PASSWORD_KEY0;
DcsmZ1Regs.Z1_CSMKEY1 = PASSWORD_KEY1;
DcsmZ1Regs.Z1_CSMKEY2 = PASSWORD_KEY2;
DcsmZ1Regs.Z1_CSMKEY3 = PASSWORD_KEY3;
}
for secure (force bit in Z1_CR)
void SecureMemory()
{
EALLOW;
DcsmZ1Regs.Z1_CR.bit.FORCESEC = 1;
EDIS;
}
for test purpose , i have called UnsecureMemory() from the application , and then connect with JTAG and watch Z1_CR
it was all 0 , i expcted to see UNSECURE at 1 , but it wasnt the case , as if the functino doesnt prefrom PMF , please advise