Does one need to connect VREFHI and VREFLO pins on the 28035 if planning to use the internal reference?
It is not clear to me from the data sheet if they are internally connected or not.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does one need to connect VREFHI and VREFLO pins on the 28035 if planning to use the internal reference?
It is not clear to me from the data sheet if they are internally connected or not.
VREFLO is used, VREFHI is not. VREFLO needs to be connected to VSSA in this mode; VREFHI should be tied off to VDDA for safest option(technically it could be floated). This is only valid on 80 pin, 64 pin VREFLO is tied off internally to VSSA.
I agree that there is not a good/concise statement regarding this in the DS(will look to add something here), but this is clarified in the ADC UG:
http://focus.ti.com/lit/ug/spruge5b/spruge5b.pdf
Sect 1.9.1.
Best,
Matthew