Part Number: TMS320F280049
Other Parts Discussed in Thread: AFE031, OPA521
Hi,
a customer was looking at the PLC PHY implementation with the AFE031, where the C2000 device is using precise PWM to generate the fundamental frequencies for FSK based PLC.
http://www.ti.com/lit/an/sprac94c/sprac94c.pdf
The customer was wondering if it is possible with the new F280049 to use the 12-bit buffered DAC which can achieve max 500 ksps, to actually generate the sine waves as inputs to the AFE031. is this possible?
Thanks!
--Gunter