Other Parts Discussed in Thread: SN65HVD230
#include "DSP2803x_Device.h" // DSP28 Headerfile Include File
#include "DSP2803x_Examples.h" // DSP28 Examples Include File
void initmaster(void) // Initialize eCAN-A module
{
struct ECAN_REGS ECanaShadow;
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // Configure GPIO30 for CANRXA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // Configure GPIO31 for CANTXA operation
/// EDIS;
/* Create a shadow register structure for the CAN control registers. This is
needed, since only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents or return
false data. */
/// EALLOW; // EALLOW enables access to protected bits
/* Configure eCAN RX and TX pins for CAN operation using eCAN regs*/
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
/* Configure eCAN for HECC mode - (reqd to access mailboxes 16 thru 31) */
// HECC mode also enables time-stamping feature
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Initialize all bits of 'Message Control Register' to zero */
// Some bits of MSGCTRL register come up in an unknown state. For proper operation,
// all bits (including reserved bits) of MSGCTRL must be initialized to zero
ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */
ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
/* Configure bit timing parameters for eCANA*/
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
/* The following block is only for 60 MHz SYSCLKOUT. (30 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */
ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 6;
ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
/// EDIS;
ECanaMboxes.MBOX0.MSGID.all = 0x80000000;//0x9555AAA0;
ECanaMboxes.MBOX1.MSGID.all = 0x80000001;//0x9555AAA1;
ECanaMboxes.MBOX2.MSGID.all = 0x80000002;//0x9555AAA2;
ECanaMboxes.MBOX3.MSGID.all = 0x80000003;//0x9555AAA3;
ECanaMboxes.MBOX4.MSGID.all = 0x80000004;//0x9555AAA4;
ECanaMboxes.MBOX5.MSGID.all = 0x80000005;//0x9555AAA5;
ECanaMboxes.MBOX6.MSGID.all = 0x80000006;//0x9555AAA6;
ECanaMboxes.MBOX7.MSGID.all = 0x80000007;//0x9555AAA7;
ECanaMboxes.MBOX8.MSGID.all = 0x80000008;//0x9555AAA8;
ECanaMboxes.MBOX9.MSGID.all = 0x80000009;//0x9555AAA9;
ECanaMboxes.MBOX10.MSGID.all = 0x8000000a;//0x9555AAAA;
ECanaMboxes.MBOX11.MSGID.all = 0x8000000b;//0x9555AAAB;
ECanaMboxes.MBOX12.MSGID.all = 0x8000000c;//0x9555AAAC;
ECanaMboxes.MBOX13.MSGID.all = 0x8000000d;//0x9555AAAD;
ECanaMboxes.MBOX14.MSGID.all = 0x8000000e;//0x9555AAAE;
ECanaMboxes.MBOX15.MSGID.all = 0x8000000f;//0x9555AAAF;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanaMboxes.MBOX16.MSGID.all = 0x81111110;//0x9555AAA0;
ECanaMboxes.MBOX17.MSGID.all = 0x81111111;//0x9555AAA1;
ECanaMboxes.MBOX18.MSGID.all = 0x81111112;//0x9555AAA2;
ECanaMboxes.MBOX19.MSGID.all = 0x81111113;//0x9555AAA3;
ECanaMboxes.MBOX20.MSGID.all = 0x81111114;//0x9555AAA4;
ECanaMboxes.MBOX21.MSGID.all = 0x81111115;//0x9555AAA5;
ECanaMboxes.MBOX22.MSGID.all = 0x81111116;//0x9555AAA6;
ECanaMboxes.MBOX23.MSGID.all = 0x81111117;//0x9555AAA7;
ECanaMboxes.MBOX24.MSGID.all = 0x81111118;//0x9555AAA8;
ECanaMboxes.MBOX25.MSGID.all = 0x81111119;//0x9555AAA9;
ECanaMboxes.MBOX26.MSGID.all = 0x8111111a;//0x9555AAAA;
ECanaMboxes.MBOX27.MSGID.all = 0x8111111b;//0x9555AAAB;
ECanaMboxes.MBOX28.MSGID.all = 0x8111111c;//0x9555AAAC;
ECanaMboxes.MBOX29.MSGID.all = 0x8111111d;//0x9555AAAD;
ECanaMboxes.MBOX30.MSGID.all = 0x8111111e;//0x9555AAAE;
ECanaMboxes.MBOX31.MSGID.all = 0x8111111f;//0x9555AAAF;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0xFFFF0000;
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0xFFFFFFFF;
// Specify that 8 bits will be sent/received
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 4;//8;
// Write to the mailbox RAM field of MBOX0 - 15
ECanaMboxes.MBOX0.MDL.all = 0x12345678;
ECanaMboxes.MBOX0.MDH.all = 0x13579ace;
ECanaMboxes.MBOX1.MDL.all = 0x11111111;
ECanaMboxes.MBOX1.MDH.all = 0x11111111;
ECanaMboxes.MBOX2.MDL.all = 0x22222222;
ECanaMboxes.MBOX2.MDH.all = 0x22222222;
ECanaMboxes.MBOX3.MDL.all = 0x33333333;
ECanaMboxes.MBOX3.MDH.all = 0x33333333;
ECanaMboxes.MBOX4.MDL.all = 0x44444444;
ECanaMboxes.MBOX4.MDH.all = 0x44444444;
ECanaMboxes.MBOX5.MDL.all = 0x55555555;
ECanaMboxes.MBOX5.MDH.all = 0x55555555;
ECanaMboxes.MBOX6.MDL.all = 0x66666666;
ECanaMboxes.MBOX6.MDH.all = 0x66666666;
ECanaMboxes.MBOX7.MDL.all = 0x77777777;
ECanaMboxes.MBOX7.MDH.all = 0x77777777;
ECanaMboxes.MBOX8.MDL.all = 0x88888888;
ECanaMboxes.MBOX8.MDH.all = 0x88888888;
ECanaMboxes.MBOX9.MDL.all = 0x99999999;
ECanaMboxes.MBOX9.MDH.all = 0x99999999;
ECanaMboxes.MBOX10.MDL.all = 0xaaaaaaaa;
ECanaMboxes.MBOX10.MDH.all = 0xaaaaaaaa;
ECanaMboxes.MBOX11.MDL.all = 0xbbbbbbbb;
ECanaMboxes.MBOX11.MDH.all = 0xbbbbbbbb;
ECanaMboxes.MBOX12.MDL.all = 0xcccccccc;
ECanaMboxes.MBOX12.MDH.all = 0xcccccccc;
ECanaMboxes.MBOX13.MDL.all = 0xdddddddd;
ECanaMboxes.MBOX13.MDH.all = 0xdddddddd;
ECanaMboxes.MBOX14.MDL.all = 0xeeeeeeee;
ECanaMboxes.MBOX14.MDH.all = 0xeeeeeeee;
ECanaMboxes.MBOX15.MDL.all = 0xffffffff;
ECanaMboxes.MBOX15.MDH.all = 0xffffffff;
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
/// EALLOW;
/// ECanaRegs.CANMIM.all = 0xFFFFFFFF;
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
/// EALLOW;
/// ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
/// ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
/// ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/// EDIS;
}
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
void main(void)
{
// struct ECAN_REGS ECanaShadow;
InitSysCtrl();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
setcanm(); // Initialize eCAN-A module
for(;;)
{
ECanaRegs.CANTRS.all = 0x0000FFFF; // Set TRS for all transmit mailboxes
while(ECanaRegs.CANTA.all != 0x0000FFFF ) {} // Wait for all TAn bits to be set..
ECanaRegs.CANTA.all = 0x0000FFFF; // Clear all TAn
}
}
#include "DSP2803x_Device.h" // DSP28 Headerfile Include File
#include "DSP2803x_Examples.h" // DSP28 Examples Include File
void initslave(void) // Initialize eCAN-A module
{
struct ECAN_REGS ECanaShadow;
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // Configure GPIO30 for CANRXA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // Configure GPIO31 for CANTXA operation
/// EDIS;
/* Create a shadow register structure for the CAN control registers. This is
needed, since only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents or return
false data. */
/// EALLOW; // EALLOW enables access to protected bits
/* Configure eCAN RX and TX pins for CAN operation using eCAN regs*/
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
/* Configure eCAN for HECC mode - (reqd to access mailboxes 16 thru 31) */
// HECC mode also enables time-stamping feature
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Initialize all bits of 'Message Control Register' to zero */
// Some bits of MSGCTRL register come up in an unknown state. For proper operation,
// all bits (including reserved bits) of MSGCTRL must be initialized to zero
ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */
ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
/* Configure bit timing parameters for eCANA*/
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
/* The following block is only for 60 MHz SYSCLKOUT. (30 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */
ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 6;
ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
/// EDIS;
ECanaMboxes.MBOX0.MSGID.all = 0x80000000;//0x9555AAA0;
ECanaMboxes.MBOX1.MSGID.all = 0x80000001;//0x9555AAA1;
ECanaMboxes.MBOX2.MSGID.all = 0x80000002;//0x9555AAA2;
ECanaMboxes.MBOX3.MSGID.all = 0x80000003;//0x9555AAA3;
ECanaMboxes.MBOX4.MSGID.all = 0x80000004;//0x9555AAA4;
ECanaMboxes.MBOX5.MSGID.all = 0x80000005;//0x9555AAA5;
ECanaMboxes.MBOX6.MSGID.all = 0x80000006;//0x9555AAA6;
ECanaMboxes.MBOX7.MSGID.all = 0x80000007;//0x9555AAA7;
ECanaMboxes.MBOX8.MSGID.all = 0x80000008;//0x9555AAA8;
ECanaMboxes.MBOX9.MSGID.all = 0x80000009;//0x9555AAA9;
ECanaMboxes.MBOX10.MSGID.all = 0x8000000a;//0x9555AAAA;
ECanaMboxes.MBOX11.MSGID.all = 0x8000000b;//0x9555AAAB;
ECanaMboxes.MBOX12.MSGID.all = 0x8000000c;//0x9555AAAC;
ECanaMboxes.MBOX13.MSGID.all = 0x8000000d;//0x9555AAAD;
ECanaMboxes.MBOX14.MSGID.all = 0x8000000e;//0x9555AAAE;
ECanaMboxes.MBOX15.MSGID.all = 0x8000000f;//0x9555AAAF;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanaMboxes.MBOX16.MSGID.all = 0x81111110;//0x9555AAA0;
ECanaMboxes.MBOX17.MSGID.all = 0x81111111;//0x9555AAA1;
ECanaMboxes.MBOX18.MSGID.all = 0x81111112;//0x9555AAA2;
ECanaMboxes.MBOX19.MSGID.all = 0x81111113;//0x9555AAA3;
ECanaMboxes.MBOX20.MSGID.all = 0x81111114;//0x9555AAA4;
ECanaMboxes.MBOX21.MSGID.all = 0x81111115;//0x9555AAA5;
ECanaMboxes.MBOX22.MSGID.all = 0x81111116;//0x9555AAA6;
ECanaMboxes.MBOX23.MSGID.all = 0x81111117;//0x9555AAA7;
ECanaMboxes.MBOX24.MSGID.all = 0x81111118;//0x9555AAA8;
ECanaMboxes.MBOX25.MSGID.all = 0x81111119;//0x9555AAA9;
ECanaMboxes.MBOX26.MSGID.all = 0x8111111a;//0x9555AAAA;
ECanaMboxes.MBOX27.MSGID.all = 0x8111111b;//0x9555AAAB;
ECanaMboxes.MBOX28.MSGID.all = 0x8111111c;//0x9555AAAC;
ECanaMboxes.MBOX29.MSGID.all = 0x8111111d;//0x9555AAAD;
ECanaMboxes.MBOX30.MSGID.all = 0x8111111e;//0x9555AAAE;
ECanaMboxes.MBOX31.MSGID.all = 0x8111111f;//0x9555AAAF;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0x0000FFFF;
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0xFFFFFFFF;
// Specify that 8 bits will be sent/received
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 4;//8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 4;//8;
}
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
void mailbox_chec(int32 T1, int32 T2, int32 T3);
void mailbox_rea(int16 i);
// Global variable for this example
Uint32 ErrorCoun;
Uint32 PassCoun;
Uint32 MessageReceivedCoun;
Uint32 TestMbo1 = 0;
Uint32 TestMbo2 = 0;
Uint32 TestMbo3 = 0;
void main(void)
{
Uint16 j;
// struct ECAN_REGS ECanaShadow;
InitSysCtrl();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
MessageReceivedCoun = 0;
ErrorCoun = 0;
PassCoun = 0;
setcans(); // Initialize eCAN-A module
for(;;)
{
//Read from Receive mailboxes and begin checking for data */
for(j=0; j<16; j++) // Read & check 16 mailboxes
{
mailbox_rea(j); // This func reads the indicated mailbox data
mailbox_chec(TestMbo1,TestMbo2,TestMbo3); // Checks the received data
}
}
}
// This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr).
void mailbox_rea(int16 MBXnb)
{
volatile struct MBOX *Mailbo;
Mailbo = &ECanaMboxes.MBOX0 + MBXnb;
TestMbo1 = Mailbo->MDL.all; // = 0x9555AAAn (n is the MBX number)
TestMbo2 = Mailbo->MDH.all; // = 0x89ABCDEF (a constant)
TestMbo3 = Mailbo->MSGID.all;// = 0x9555AAAn (n is the MBX number)
} // MSGID of a rcv MBX is transmitted as the MDL data.
void mailbox_chec(int32 T1, int32 T2, int32 T3)
{
if((T1 != T3) || ( T2 != 0x89ABCDEF))
{
ErrorCoun++;
}
else
{
PassCoun++;
}
}
i have compose four files for initial and main in both side.
then i used 2 computer and 2 ICE(development board) connecting throught a IC (SN65HVD230). but i don't know why it didn't work.
can any one please help to correct my code? cuz i can't find out any wrong in it.
please.
those Filename Extensions should be exchanged into .c (not .txt)