Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hi,
I am trying to create a batch file for my new project for application-specific run time libraries. One thing I couldn't get is how to create run time libraries itself from the batch file. Attached is the batch file. Though I didn't implement the run time libraries creation. I need help with that part.
:begin ECHO Compiling %1 set FILE_NAME=%1 SET LIB_PATH=C:\Users\h352524\workspace_v9_2\F28377D_Base_SMDs\Debug\myprogram.out SET TO_COMPILE_FILES=C:\Users\h352524\workspace_v9_2\F28377D_Base_SMDs\Source\sci.c SET INCLUDE_PATH=C:\Users\h352524\workspace_v9_2\rts_TMS320F28379_Flash_Lib SET COMPILER_FLAGS= -v28 -ml --float_support=fpu32 --include_path="C:/ti/ccs920/ccs/tools/compiler/ti-cgt-c2000_18.12.3.LTS/include" --include_path="C:/ti/C2000Ware_3_01_00_00_Software/device_support/f2837xd/headers/include" --include_path="C:/ti/C2000Ware_3_01_00_00_Software/device_support/f2837xd/common/include"/ --include_path=%INCLUDE_PATH% -g --define=CPU1 --display_error_number --diag_suppress=10063 --diag_warning=225 REM set PATH=%TO_COMPILE_FILES%;%PATH% REM Description of Linker Flags REM -r link with the reolcation information SET LINKER_FLAGS=--run_linker --rom_model cl2000 %TO_COMPILE_FILES% %COMPILER_FLAGS% --include_path =%LIB_PATH% :endfile