This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fixing Piccolo ControlSTICK - Bricked

Hello,

I unplugged my piccolo controlSTICK without disconnecting it 1st from ccs. When I tried to use it again, it gives me the following message:

******************************************************

Error connecting to the target:

Error 0x80000240/-151

Fatal Error during: Initialization, OCS, 

This error was generated by TI's USCIF driver.

 

SC_ERR_POD_OPEN <-151>

This utility failed to open the adapter for a custom emulator.

The adapter returned an error.

 

 

I/O Port = 0

 

Board Name: F28027 XDS100USB

Cpu Name: TMS320C2800_0

 

Abort: Close Code Composer Studio.

Retry: Try to connect to the target again.

Cancel: Remain disconnected from the target

Diagnostic: Run diagnostic utility.

 

******************************************************

Is there anyway to "unbrick" my controlSTICK?

 

Thanks,

Alex