This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280041: PWM IO 2ms high level signal

Part Number: TMS320F280041

Tool/software: Code Composer Studio

Dear team

My customer designed their board with TMS320F280041.  ADC, PWM, and other modules could be used normally now.

But they found that the PWM IO signal must had a high level signal of about 2ms as long as the power (5V) was turned on.

They tested the example project epwm_ex2_updown_aq. It also had 2ms high level signal.

boot mode: GPIO32 high, GPIO24 high

Please help.

  • At reset, all GPIOs are in high impedance mode. The user can change them to be in GPIO Output mode with LOW state when the device comes out of reset. During the initialization of the ePWM module then can keep the GPIO in the GPIO Output mode with LOW state. When they are ready to enable the ePWM module, they can switch the GPIO to be in driven by the ePWM module. I dont believe there is an issue with the GPIO module, it should be just a matter of initialization sequence.

    Nima

  • Sorry for late reply


    This method had been tested and there still had a high level of about 2ms

    1 config the GPIO FIRST 
    GPIO_setPadConfig(2, GPIO_PIN_TYPE_OD);
    GPIO_setPinConfig(GPIO_2_GPIO2);
    GPIO_setPadConfig(3, GPIO_PIN_TYPE_OD);
    GPIO_setPinConfig(GPIO_3_GPIO3);

    2  When they are ready to enable the ePWM module, they switch the GPIO to be in driven by the ePWM module. 
    GPIO_setPadConfig(2, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_2_EPWM2A);
    GPIO_setPadConfig(3, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_3_EPWM2B);

    Please help

  • Can you try setting the pins to low state at the top of the main?

    I'm assuming another initialization is causing this.