Other Parts Discussed in Thread: SN65HVD230
i have composed the program which i want 2 dsp(tms320 f 28035) to communicate each other.
when i run it, then the one in the master always gets into trip ( while(ECanaRegs.CANTA.all != 0x0000FFFF ) ) to wait the CANTA
register changing to 1. always~~~(of course, i did wire the transceiver for ECAN, numbered SN65HVD230 )
i have tried masive times, i am nearly dying.
this problem really drives me crazy~~
can any kind rescurer help me to correct the program which Refers to attachment?
please~~~
below file's Filename Extension should be exchanged .txt into .c
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
void main(void)
{
Uint16 j;
struct ECAN_REGS ECanaShadow;
InitSysCtrl();
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // Configure GPIO30 for CANRXA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // Configure GPIO31 for CANTXA operation
EDIS;
}
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
caninit(); // Initialize eCAN-A module
// Write to the mailbox RAM field of MBOX0 - 15
ECanaMboxes.MBOX0.MDL.all = 0x12345678;
ECanaMboxes.MBOX0.MDH.all = 0x13579ace;
ECanaMboxes.MBOX1.MDL.all = 0x11111111;
ECanaMboxes.MBOX1.MDH.all = 0x11111111;
ECanaMboxes.MBOX2.MDL.all = 0x22222222;
ECanaMboxes.MBOX2.MDH.all = 0x22222222;
ECanaMboxes.MBOX3.MDL.all = 0x33333333;
ECanaMboxes.MBOX3.MDH.all = 0x33333333;
ECanaMboxes.MBOX4.MDL.all = 0x44444444;
ECanaMboxes.MBOX4.MDH.all = 0x44444444;
ECanaMboxes.MBOX5.MDL.all = 0x55555555;
ECanaMboxes.MBOX5.MDH.all = 0x55555555;
ECanaMboxes.MBOX6.MDL.all = 0x66666666;
ECanaMboxes.MBOX6.MDH.all = 0x66666666;
ECanaMboxes.MBOX7.MDL.all = 0x77777777;
ECanaMboxes.MBOX7.MDH.all = 0x77777777;
ECanaMboxes.MBOX8.MDL.all = 0x88888888;
ECanaMboxes.MBOX8.MDH.all = 0x88888888;
ECanaMboxes.MBOX9.MDL.all = 0x99999999;
ECanaMboxes.MBOX9.MDH.all = 0x99999999;
ECanaMboxes.MBOX10.MDL.all = 0xaaaaaaaa;
ECanaMboxes.MBOX10.MDH.all = 0xaaaaaaaa;
ECanaMboxes.MBOX11.MDL.all = 0xbbbbbbbb;
ECanaMboxes.MBOX11.MDH.all = 0xbbbbbbbb;
ECanaMboxes.MBOX12.MDL.all = 0xcccccccc;
ECanaMboxes.MBOX12.MDH.all = 0xcccccccc;
ECanaMboxes.MBOX13.MDL.all = 0xdddddddd;
ECanaMboxes.MBOX13.MDH.all = 0xdddddddd;
ECanaMboxes.MBOX14.MDL.all = 0xeeeeeeee;
ECanaMboxes.MBOX14.MDH.all = 0xeeeeeeee;
ECanaMboxes.MBOX15.MDL.all = 0xffffffff;
ECanaMboxes.MBOX15.MDH.all = 0xffffffff;
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
/// EALLOW;
/// ECanaRegs.CANMIM.all = 0xFFFFFFFF;
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
/// EALLOW;
/// ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
/// ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
/// ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/// EDIS;
// Begin transmitting
for(;;)
{
ECanaRegs.CANTRS.all = 0x0000FFFF; // Set TRS for all transmit mailboxes
while(ECanaRegs.CANTA.all != 0x0000FFFF ) {} // Wait for all TAn bits to be set..
ECanaRegs.CANTA.all = 0x0000FFFF; // Clear all TAn
while(ECanaRegs.CANTA.all != 0x00000000 ) {}
}
}
//===========================================================================
// No more.
//===========================================================================
#include "DSP2803x_Device.h" // DSP28 Headerfile Include File
#include "DSP2803x_Examples.h" // DSP28 Examples Include File
void caninit(void) // Initialize eCAN-A module
{
struct ECAN_REGS ECanaShadow;
EALLOW; // EALLOW enables access to protected bits
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Configure bit timing parameters for eCANA*/
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
/* The following block is only for 60 MHz SYSCLKOUT. (30 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */
ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 6;
ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
ECanaRegs.CANTRR.all=0xffffffff;
do
{
ECanaShadow.CANTRS.all = ECanaRegs.CANTRS.all;
} while(ECanaShadow.CANTRS.all != 0 );
ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */
ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
// Mailboxs can be written to 16-bits or 32-bits at a time
// Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
ECanaMboxes.MBOX0.MSGID.all = 0x80000000;
ECanaMboxes.MBOX1.MSGID.all = 0x80000001;
ECanaMboxes.MBOX2.MSGID.all = 0x80000002;
ECanaMboxes.MBOX3.MSGID.all = 0x80000003;
ECanaMboxes.MBOX4.MSGID.all = 0x80000004;
ECanaMboxes.MBOX5.MSGID.all = 0x80000005;
ECanaMboxes.MBOX6.MSGID.all = 0x80000006;
ECanaMboxes.MBOX7.MSGID.all = 0x80000007;
ECanaMboxes.MBOX8.MSGID.all = 0x80000008;
ECanaMboxes.MBOX9.MSGID.all = 0x80000009;
ECanaMboxes.MBOX10.MSGID.all = 0x8000000A;
ECanaMboxes.MBOX11.MSGID.all = 0x8000000B;
ECanaMboxes.MBOX12.MSGID.all = 0x8000000C;
ECanaMboxes.MBOX13.MSGID.all = 0x8000000D;
ECanaMboxes.MBOX14.MSGID.all = 0x8000000E;
ECanaMboxes.MBOX15.MSGID.all = 0x8000000F;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanaMboxes.MBOX16.MSGID.all = 0x81111110;
ECanaMboxes.MBOX17.MSGID.all = 0x81111111;
ECanaMboxes.MBOX18.MSGID.all = 0x81111112;
ECanaMboxes.MBOX19.MSGID.all = 0x81111113;
ECanaMboxes.MBOX20.MSGID.all = 0x81111114;
ECanaMboxes.MBOX21.MSGID.all = 0x81111115;
ECanaMboxes.MBOX22.MSGID.all = 0x81111116;
ECanaMboxes.MBOX23.MSGID.all = 0x81111117;
ECanaMboxes.MBOX24.MSGID.all = 0x81111118;
ECanaMboxes.MBOX25.MSGID.all = 0x81111119;
ECanaMboxes.MBOX26.MSGID.all = 0x8111111A;
ECanaMboxes.MBOX27.MSGID.all = 0x8111111B;
ECanaMboxes.MBOX28.MSGID.all = 0x8111111C;
ECanaMboxes.MBOX29.MSGID.all = 0x8111111D;
ECanaMboxes.MBOX30.MSGID.all = 0x8111111E;
ECanaMboxes.MBOX31.MSGID.all = 0x8111111F;
// Specify that 8 bits will be sent/received
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0xFFFF0000;
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0xFFFFFFFF;
// EDIS;
}
//---------------------------------------------------------------------------
// Example: InitECanGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as eCAN pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// Only one GPIO pin should be enabled for CANTXA operation.
// Only one GPIO pin shoudl be enabled for CANRXA operation.
// Comment out other unwanted lines.
/* Note: Bit timing parameters must be chosen based on the network parameters such as
the sampling point desired and the propagation delay of the network. The propagation
delay is a function of length of the cable, delay introduced by the
transceivers and opto/galvanic-isolators (if any).
The parameters used in this file must be changed taking into account the above mentioned
factors in order to arrive at the bit-timing parameters suitable for a network.
*/
//===========================================================================
// End of file.
//===========================================================================
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
long ffff[16]={0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
void main(void)
{
struct ECAN_REGS ECanaShadow;
InitSysCtrl();
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // Configure GPIO30 for CANRXA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // Configure GPIO31 for CANTXA operation
EDIS;
}
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
caninitsalve(); // Initialize eCAN-A module
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
/// EALLOW;
/// ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
/// ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
/// ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/// EDIS;
// Begin waiting
for(;;)
{
ffff[0] = ECanaMboxes.MBOX0.MDL.all;
ffff[1] = ECanaMboxes.MBOX1.MDL.all;
ffff[2] = ECanaMboxes.MBOX2.MDL.all;
ffff[3] = ECanaMboxes.MBOX3.MDL.all;
ffff[4] = ECanaMboxes.MBOX4.MDL.all;
ffff[5] = ECanaMboxes.MBOX5.MDL.all;
ffff[6] = ECanaMboxes.MBOX6.MDL.all;
ffff[7] = ECanaMboxes.MBOX7.MDL.all;
ffff[8] = ECanaMboxes.MBOX8.MDL.all;
ffff[9] = ECanaMboxes.MBOX9.MDL.all;
ffff[10] = ECanaMboxes.MBOX10.MDL.all;
ffff[11] = ECanaMboxes.MBOX11.MDL.all;
ffff[12] = ECanaMboxes.MBOX12.MDL.all;
ffff[13] = ECanaMboxes.MBOX13.MDL.all;
ffff[14] = ECanaMboxes.MBOX14.MDL.all;
ffff[15] = ECanaMboxes.MBOX15.MDL.all;
}
}
//===========================================================================
// No more.
//===========================================================================
#include "DSP2803x_Device.h" // DSP28 Headerfile Include File
#include "DSP2803x_Examples.h" // DSP28 Examples Include File
//---------------------------------------------------------------------------
// InitECan:
//---------------------------------------------------------------------------
// This function initializes the eCAN module to a known state.
//
void caninitsalve(void) // Initialize eCAN-A module
{
struct ECAN_REGS ECanaShadow;
EALLOW; // EALLOW enables access to protected bits
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Configure bit timing parameters for eCANA*/
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
/* The following block is only for 60 MHz SYSCLKOUT. (30 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */
ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 6;
ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
//`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',`,',
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
/// ECanaRegs.CANTRR.all=0xffffffff;
/// do
/// {
/// ECanaShadow.CANTRS.all = ECanaRegs.CANTRS.all;
/// } while(ECanaShadow.CANTRS.all != 0 );
ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */
ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
// Mailboxs can be written to 16-bits or 32-bits at a time
// Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
ECanaMboxes.MBOX0.MSGID.all = 0x81111110;
ECanaMboxes.MBOX1.MSGID.all = 0x81111111;
ECanaMboxes.MBOX2.MSGID.all = 0x81111112;
ECanaMboxes.MBOX3.MSGID.all = 0x81111113;
ECanaMboxes.MBOX4.MSGID.all = 0x81111114;
ECanaMboxes.MBOX5.MSGID.all = 0x81111115;
ECanaMboxes.MBOX6.MSGID.all = 0x81111116;
ECanaMboxes.MBOX7.MSGID.all = 0x81111117;
ECanaMboxes.MBOX8.MSGID.all = 0x81111118;
ECanaMboxes.MBOX9.MSGID.all = 0x81111119;
ECanaMboxes.MBOX10.MSGID.all = 0x8111111A;
ECanaMboxes.MBOX11.MSGID.all = 0x8111111B;
ECanaMboxes.MBOX12.MSGID.all = 0x8111111C;
ECanaMboxes.MBOX13.MSGID.all = 0x8111111D;
ECanaMboxes.MBOX14.MSGID.all = 0x8111111E;
ECanaMboxes.MBOX15.MSGID.all = 0x8111111F;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanaMboxes.MBOX16.MSGID.all = 0x80000000;
ECanaMboxes.MBOX17.MSGID.all = 0x80000001;
ECanaMboxes.MBOX18.MSGID.all = 0x80000002;
ECanaMboxes.MBOX19.MSGID.all = 0x80000003;
ECanaMboxes.MBOX20.MSGID.all = 0x80000004;
ECanaMboxes.MBOX21.MSGID.all = 0x80000005;
ECanaMboxes.MBOX22.MSGID.all = 0x80000006;
ECanaMboxes.MBOX23.MSGID.all = 0x80000007;
ECanaMboxes.MBOX24.MSGID.all = 0x80000008;
ECanaMboxes.MBOX25.MSGID.all = 0x80000009;
ECanaMboxes.MBOX26.MSGID.all = 0x8000000A;
ECanaMboxes.MBOX27.MSGID.all = 0x8000000B;
ECanaMboxes.MBOX28.MSGID.all = 0x8000000C;
ECanaMboxes.MBOX29.MSGID.all = 0x8000000D;
ECanaMboxes.MBOX30.MSGID.all = 0x8000000E;
ECanaMboxes.MBOX31.MSGID.all = 0x8000000F;
// Specify that 8 bits will be sent/received
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0x0000FFFF;
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0xFFFFFFFF;
// EDIS;
}
//---------------------------------------------------------------------------
// Example: InitECanGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as eCAN pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// Only one GPIO pin should be enabled for CANTXA operation.
// Only one GPIO pin shoudl be enabled for CANRXA operation.
// Comment out other unwanted lines.
/* Note: Bit timing parameters must be chosen based on the network parameters such as
the sampling point desired and the propagation delay of the network. The propagation
delay is a function of length of the cable, delay introduced by the
transceivers and opto/galvanic-isolators (if any).
The parameters used in this file must be changed taking into account the above mentioned
factors in order to arrive at the bit-timing parameters suitable for a network.
*/
//===========================================================================
// End of file.
//===========================================================================