This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error while launching in target...

 Dear all,

              While debugging the application code into the target the following two errors are coming. Try to help me in rectifying it.

Error 1:

         Exception occured during launch

        Reason: Failed to initialize debug server

        Reason: Cannot read system setup data from XML file C:\Documents and Settings\psk\user\CCSTargetConfigurations\NewTargetConfiguration.ccxml

                        Unable save system setup information,can't write to file

Error 2:

        Multiple operations have reported errors.Select an error to view its details.

        Asynchronous viewer update(Time of error............)

       Asynchronous viewer update(Time of error............)

 

I'm using 28035 experimenter's kit and CCS V4.2.1

 

Regards,

Saravanakumar...