Part Number: TMS320F28379D
Greetings,
I am looking at the documentation for the Peripheral Signal Multiplexer (table 26-3). It indicates that EPWM1,PWMA can be replaced with CLB1.CLB1_OUT0_0 using the mux. According to Table 8-7 GPIO Muxed Pins, EPWM1A goes to both GPIO0 and GPIO145. When CLB1.CLB1_OUT0_0 is muxed out via the Peripheral Signal Multiplexer, does it go to both pins too or only to one of those?
Thank you,
Ed