This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Input Resistance Model for GPIO in 28022

`

  • Andrew,

    Assuming the output buffer is not turned on you have a very high input impedance - probably in the Mohms range - discounting the pullup/down circuit. The pulls are active circuits so the specs are given in terms of current source/sink, not resistance. These numbers are in the datasheet (section 6.3 - pullups are typically around -140uA). The input capacitance is given in this same section (typ 2pF). This is pretty much it.

    Regards,
    Dave Foley