Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Hello,
I'm developing an application that uses all three cores in an F28388D. I've used Sysconfig to create peripheral initialization files for the CPU1 project in CCS, and I can link to the board.h file from the CPU2 project so I can use the same defined names for the peripherals. But that causes errors if I try to include it in the CM project because board.h includes the file device.h, which ultimately tries to include header files for the C28x driverlib. (Which are not on the CM project's include path, thus causing the compile to fail.)
Is there a way for the CM project to use Sysconfig's definitions without having to create a separate include file by hand?
Dave