Other Parts Discussed in Thread: CONTROLSUITE
I am using the F28027 from the Piccolo controlStick development kit and CCS4 environment.
There is an external 6MHz crystal and an associated on chip oscillator available. I am able to switch on this oscillator. But so far I am not successful to drive the system clock / PLL (SYSCLKOUT) with it. The processor switches back to internal 10MHz OSC1 as soon as I finally set bit OSCCLKSRCSEL in register CLKCTL. I have found no hint in the documentation which states that this task is not allowed. Maybe there is a special sequence (or timing between instructions) necessary to get that switching done?
I apprechiate any help!
Roland