Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I am using the development board LAUNCHXL-F28379D. I would like to configure an external interrupt using GPIO pin 67. I have set the GPIO67 pin though the Input X-Bar to Input 6 for XINT3. I have also enabled the PIEIER12 bit INTx1 and IER bit INT12 . However, the interrupt is not entered into/generated when I put the GPIO pin to 3V.
Any help would be really appreciated.
Thanks
Dan