This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: SPI example, getting data from ADS8920(SPI output)

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hi, I want to ask about the SPI example.

I want to get some data from ADS8920 which gives SPI digital output.

So, I want to know some examples if you guys know some examples about.

Please let me know.

I think TI only offer loopback example....

Best wishes,

  • Ming,

    We don't have an example code / library which you can use to directly interface with ADS8920.

    It is true that SPI example code which we have in C2000Ware are loopback examples. But, we have 3 different flavors of SPI examples which can be modified to suit one application. The reason we have loopback code is to have the SPI code run standalone without the need to have a slave SPI.

    Please refer to F2837xD_DEV_USER_GUIDE.pdf to to know about the details of each example code provided.

    Regards,

    Manoj