Imagine i configured the ePWM1A and configured ePWM1B be complimentary of ePWM1A.
Question 1
if i set the bits such that during Trip Signal event ePWM1A pin to be low. what would be state of ePWM1B pin during trip signal event.
Will it be low or high or it will continue the state it was before?
Question 2
Any restriction to minimum duty cycle.
If set the duty cycle of PWM to be zero on the epWM1A can i expect epWM1B to be high always ?