Part Number: TMS320F28388S
Other Parts Discussed in Thread: C2000WARE
Hi Team,
My customer want to configure 60Mhz clock for USB at F28388, from the TRM that the clock source for USB is either CMCLK or CPU1.SYSCLK, but they require that CMCLK is configure to 125MHz, and CPU1.SYSCLK is configure to 200MHz, in this case how to configure 60MHz clock for USB?
Set up the auxiliary PLL so a 60 MHz output clock is provided to the USB module. This fixed frequency is
required for all USB operations. See the System Control chapter for more details.