This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

controlSUITE FLASH issue

Other Parts Discussed in Thread: CONTROLSUITE

Hi TI Gurus.

Found some issues whilest working with the controlSUITE Flash stuff for Piccolo A

  1. the include files in the folder ..\controlSUITE\libs\utilities\flash_api\f2802x\v201\include are wrong. They should be Flash2802x_API_Library.h and Flash2802x_API_Config.h instead (It is not just the name that is wrong, content should be different too)
  2. In the File ..\controlSUITE\device_support\f2802x\v128\DSP2802x_common\source\DSP2802x_SysCtrl.c you have a method called InitFlash(). In the compile switch you forgot to include the 50MHz devices.

BR Andreas

  • andreas von kaenel said:

    Hi TI Gurus.

    Found some issues whilest working with the controlSUITE Flash stuff for Piccolo A

    1. the include files in the folder ..\controlSUITE\libs\utilities\flash_api\f2802x\v201\include are wrong. They should be Flash2802x_API_Library.h and Flash2802x_API_Config.h instead (It is not just the name that is wrong, content should be different too)
    2. In the File ..\controlSUITE\device_support\f2802x\v128\DSP2802x_common\source\DSP2802x_SysCtrl.c you have a method called InitFlash(). In the compile switch you forgot to include the 50MHz devices.

    BR Andreas

    Thank you for reporting this Andreas - I will feed it back to the team for correction.

     

    Cheers

    Lori