This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: Filesystem for an SPI NOR Flash using sysbios

Part Number: TMS320F28374S
Other Parts Discussed in Thread: C2000WARE

Hello expert.

We are developing a project that is based on the TMS320F28374S microprocessor, and that uses the TI operating system.

Connected to the microcontroller, via SPI, there is a nor flash memory, which we would like to manage with a filesystem.

Unfortunately, only the sys-bios is available for the C2000 family.

Is the module supplied with TI RTos that manages the flash memory file system also available for the c2000 platform? Can it be used together with the SYS-bios?

If not, does TI provide any solution for managing the filesystem in the external flash?

Thank you very much

Paolo