Hello Everyone
I use the three XINT and they are working. My configuration looks like this for GPIO2 and XINT1:
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO2 = 0;
GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL = 2;
GpioCtrlRegs.GPAQSEL1.bit.GPIO2 = 0;
EDIS;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEIER1.bit.INTx4 = 1;
IER |= M_INT1;
XIntruptRegs.XINT1CR.bit.POLARITY = 1;
XIntruptRegs.XINT1CR.bit.ENABLE = 1;
EINT;
ERTM;
I also remapped the Interrupt and at the beginning the GPIO2 is LOW. If I pull it HIGH the interrupts is released.
My problem is, that if I set a breakpoint at the beginning of the interrupt I can see it released when the GPIO is set HIGH. But it is released a second time when the GPIO2 goes back from HIGH-->LOW. I thought with the Polarity bit i set Interrupt generated on a rising edge???
Can someone tell me what I disregarded?
Kind regards
Christian