This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / F28M35H52C: F28M35H52C1 Ethernet communication problems

Part Number: F28M35H52C


Tool/software: Code Composer Studio

Hi there,

I programed unet_uip_m3 example into the Control card of TI. used static IP 169.254.254.169  (Mask: 255.255.0.0).my computer IP 169.254.254.168(Mask: 255.255.0.0).  ping via cmd and browser call to 169.254.254.169 fail . 

crossover eth cable to H52C1 control card (checked with other notebook ok). Using a previously used program still won't connect。

What is the problem here? Is it set up in the program? (This board can be connected to Ethernet before) Please help me, thank you!

best regard

Fulei Shang