Part Number: DRV8301-69M-KIT
Tool/software: Code Composer Studio
Hello,
when performing the motor(BLDC) identification using the lab 2a/b the inductance (Ls) value is varying from 20% to 30%. Is there any issue in the identification or its good to go with the variation of 20% to 30%. There is no much variation in Rs or flux values.
Rs = 0.02 ohms
Flux = 0.131 V/Hz
variation of Ls = 0.000090 H
Ls = 0.000055 H
Ls = 0.0000102 H
And, In this which value we can prefer for Ls.
Thanks
Vivishekh