Part Number: TMS320F28335
Hello,
I have been going through eCAN manual and the manual says: "It is not possible to achieve a direct digital loopback externally by connecting the CANTX and CANRX pins together (as is possible with SCI/SPI/McBSP modules). An internal loopback is possible in the self-test mode (STM)."
I have three doubts:
1. STM is internal loopback within the same CAN module, where the CAN module generates its own ACK signal, right?
2. When the manual says, external loopback is not possible, what does it mean?
Does it mean this: Communication within the same eCANA module by externally connecting the 2 pins is not possible but communication between the 2 modules present in the board: eCANA and eCANB is possible, though this is also called loopback? Or does it mean something else?
3. Why is the external loopback not possible for CAN?
Thanks,
Anu