This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049: Not enough space for Cla1Prog

Part Number: TMS320F280049


Tool/software: Code Composer Studio

Hello,

I'm working in a project using 3 cla tasks, when the code reached an important size, I started having the error: "not enough memory" for Cla1Prog, so I changed the size of RAMLS0 in the linker command file from 0x800 to 0xE50 and changed RAMLS1 accordingly reducing its size. Now the program can be compiled and copied to the f280049 flash but the cla isn't running, I gave a bigger size to RAMLS1 reducing RAMLS2 since RAMLS1 is the scratchpad but cla is not working yet, if I comment the code in one of the 3 cla tasks, the cla runs but I haven been able to get the cla running for the 3 of them.

what could be happening? am I doing something wrong?

Thanks for your help