Part Number: TMS320F28035
Hi Expert,
My customer just meets an issue after lightning surge tests, that
- the software could download to chip with emulator.
- all ADC channels sample value is 4096, even the ADC pin connect with pull down resistance, and the issue has happened twice.
- the ADC channels mainly simple input voltage, inductor current, bus voltage of H bridge PFC.
- when connect a 2ohm resistance between digital ground and analog ground, the issue could be avoided. But in normal condition, such as with 50% load, the chip is reset.
Our confusions are,
- what kind of factors could only damage the ADC module, but not the whole chip?
- what do you think of the debug method that increasing the resistance between digital and analog ground?
Customer hopes to find some opinions to debug with this issue, could you help with this? Thanks!
Best Regards
Rayna