This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 PLL and jitter

I'm currently working on a ultra real-time process, I need to measure a  velocity with extremly high accuracy. Thus, I'm preoccuped about the jitter of the onchip PLL. Since the XCLKIN maximum frequency input is 150MHz for the C28346, I can't work at 300MHz if I use an external PLL. 

As a clock source, I use a very precise OCXO. 

What is the jitter of the internal PLL? 

Thank you in advance, 

Yves Chevallier