This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Multiple CMPSS issue

Part Number: TMS320F280049C

Hello,

With 280049, we want to monitor several analog inputs to trig the EPwm with the comparators.

For instance, we have started with 2 comparators (1 and 3) and we'll set the 7.

The problem we faced is :

CMPSS1 works fine and trig the Epwm

CMPSS3 works fine when CMPSS1 is not enabled, it triggers the Epwm and an external IO

As soon as I enable CMPSS1, CMPSS3 is not working any more.

I've joined the 2 initializations pieces of code but I don't see in CMPSS1 which instructions could stuck CMPSS3 ?

Best regards

francois 

void Comp1Init(void)
{
//! Initialize Output voltage comparator.
//!
//! \param None.
//!
//! CMPSS1
//!
//! \return 0 None.
EALLOW;
CpuSysRegs.PCLKCR14.bit.CMPSS1 = 1; /* 1: Module clock is turned-on. */
Cmpss1Regs.COMPCTL.bit.COMPDACE = 1; /* 1 Comparator/DAC enabled */
/* Comparator High */
Cmpss1Regs.COMPCTL.bit.COMPHSOURCE = 0; /* 0 Inverting input of comparator driven by internal DAC */
Cmpss1Regs.COMPDACCTL.bit.SELREF = 0; /* 0 VDDA is the voltage reference for the DAC */
Cmpss1Regs.DACHVALS.bit.DACVAL = 2048;//3560;
Cmpss1Regs.COMPCTL.bit.CTRIPHSEL = 0; /* 0 Asynchronous comparator output drives CTRIPH */
//Cmpss1Regs.COMPCTL.bit.CTRIPOUTHSEL = 0; /* 0 Asynchronous comparator output drives CTRIPOUTH */
/* Input high = A2 */
AnalogSubsysRegs.CMPHPMXSEL.bit.CMP1HPMXSEL = 0; /* 0 : A2 High Positive */
/* Trip zone on EPwmA */
EPwmXbarRegs.TRIP4MUX0TO15CFG.bit.MUX0 = 0; /* Configure TRIP4 to be CTRIP1H */
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX0 = 1; /* 1: Respective output of Mux0 is enabled to drive the TRIP4 of EPWM-XBAR */
EDIS;
}

void Comp3Init(void)
{
//! Initialize Output voltage comparator.
//!
//! \param None.
//!
//! CMPSS3
//!
//! \return 0 None.
EALLOW;
CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1; /* 1: Module clock is turned-on. */
Cmpss3Regs.COMPCTL.bit.COMPDACE = 1; /* 1 Comparator/DAC enabled */
/* Comparator High */
Cmpss3Regs.COMPCTL.bit.COMPHSOURCE = 0; /* 0 Inverting input of comparator driven by internal DAC */
Cmpss3Regs.COMPDACCTL.bit.SELREF = 0; /* 0 VDDA is the voltage reference for the DAC */
Cmpss3Regs.DACHVALS.bit.DACVAL = 2048;//3560;
Cmpss3Regs.COMPCTL.bit.CTRIPHSEL = 0; /* 0 Asynchronous comparator output drives CTRIPH */
Cmpss3Regs.COMPCTL.bit.CTRIPOUTHSEL = 0; /* 0 Asynchronous comparator output drives CTRIPOUTH */
/* Input high = B3 */
AnalogSubsysRegs.CMPHPMXSEL.bit.CMP3HPMXSEL = 3; /* 3 : B3 High Positive */
/* Trip zone on EPwmA */
EPwmXbarRegs.TRIP7MUX0TO15CFG.bit.MUX4 = 0; /* Configure TRIP7 to be CTRIP3H */
EPwmXbarRegs.TRIP7MUXENABLE.bit.MUX4 = 1; /* 1: Respective output of Mux0 is enabled to drive the TRIP7 of EPWM-XBAR */
/* Output to pin */
OutputXbarRegs.OUTPUT5MUX0TO15CFG.bit.MUX4 = 0; /* 00 : Select .0 input for Mux0 */
OutputXbarRegs.OUTPUT5MUXENABLE.bit.MUX4 = 1; /* 1: Respective output of Mux0 is enabled to drive the OUTPUT5 of OUTPUT-XBAR */
GpioCtrlRegs.GPADIR.bit.GPIO28 = 1; /* 1: The pin is an output */
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1;
GpioCtrlRegs.GPAGMUX2.bit.GPIO28 = 1;
EDIS;
}

  • When you say "CMPSS3 is not working any more," is it both the output on GPIO28 and the trip of PWM that stop working or is it just one or the other? Do the COMPSTS registers show the correct status? Can you elaborate?

    Nothing in the code is jumping out at me as an issue. Do you mind sharing the part of your PWM configuration related to the trip configuration?

    Whitney

  • Hello Whitney,

    Thank you to take care of our issue.

    When CMPSS3 is alone, Both GPIO28 and Epwm trip together

    Further to your information, I've made some experiments without and with Comp1Init()

    < or > is the comparator condition

                          1    3 COMPSTS1  COMPSTS3 GPIO28 EPwm 

    CMPSS1 Set 
                          <  < 0x0300           0x0000          0           OK
                          >  < 0x0303           0x0000          0           NO
                          < > 0x0302            0x0000          0           OK
                          > > 0x0303           0x0000           0           NO
    CMPSS1 Removed 
                         < < 0x0000             0x0300         0            OK
                         > < 0x0000             0x0300         0            OK
                         < > 0x0000             0x0303         1            NO
    Here is the part of code (only for TZ in EPwm)
    (We stop 6 Epwm together so the init is indexed)
    /* Trip Zone regs (TZ) */
    EPwmRegs[n].TZCTL.bit.TZA = 2;                    /* 10 : Force EPWMxA to a low state */
    EPwmRegs[n].TZFRC.bit.OST = 1;                    /* 1 : Forces a one-shot trip event and sets the TZFLG[OST] bit. */
    /* Trip zone on Cmpss */
    EPwmRegs[n].DCTRIPSEL.bit.DCAHCOMPSEL = 0x0F;     /* 1111: Trip combination input (all trip inputs selected by DCAHTRIPSEL register ORed together) */
    EPwmRegs[n].DCAHTRIPSEL.bit.TRIPINPUT4 = 1;       /* 1: Trip Input 4 selected as combinational ORed input to DCAH mux */
    EPwmRegs[n].DCAHTRIPSEL.bit.TRIPINPUT7 = 1;       /* 1: Trip Input 7 selected as combinational ORed input to DCAH mux */
    EPwmRegs[n].TZDCSEL.bit.DCAEVT1 = 2;                /* Digital Compare Output A Event 1 Selection 010: DCAH = high, DCAL = don't care */
    EPwmRegs[n].DCACTL.bit.EVT1SRCSEL = 0;              /* 0: Source Is DCAEVT1 Signal */
    EPwmRegs[n].DCACTL.bit.EVT1FRCSYNCSEL = 1;          /* 1: Source is passed through asynchronously */
    EPwmRegs[n].TZSEL.bit.DCAEVT1 = 1;                  /* 1: Enable DCBEVT1 as one-shot-trip source for this ePWM module. */
    EDIS;
    Best regards,
    francois
  • Hi Francois,

    For debugging purposes, let's try to isolate the comparator and epwm connection for now and concentrate only on the comparator. If you route CMPSS1 and CMPSS3 only to output XBARs, do they work as intended when initialized together and separately?

  • Hello Frank,

    Thanks for you reply. I've investigate a little more on comparators but I prefer to have your opinion ?

    I've Added a small delay between turning on clock and configuration and thing are working now.

    Here is what I've Added, now CMPSS seems to be initialized correctly.

    void Comp3Init(void)
    {
    //! Initialize Output voltage comparator.
    //!
    //! \param None.
    //!
    //! CMPSS3
    //!
    //! \return 0 None.
    uchar i;
    EALLOW;
    CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1;               /* 1: Module clock is turned-on. */
    i = 0;
    do
      i ++;
    while (i != 0);
    Cmpss3Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    /* Comparator High */
    Cmpss3Regs.COMPCTL.bit.COMPHSOURCE = 0;           /* 0 Inverting input of comparator driven by internal DAC */
    Cmpss3Regs.COMPDACCTL.bit.SELREF = 0;             /* 0 VDDA is the voltage reference for the DAC */
    Cmpss3Regs.DACHVALS.bit.DACVAL = 2048;//DataFlash.VOutMax * VOUTGAIN;
    Cmpss3Regs.COMPCTL.bit.CTRIPHSEL = 0;             /* 0 Asynchronous comparator output drives CTRIPH */
    Cmpss3Regs.COMPCTL.bit.CTRIPOUTHSEL = 0;          /* 0 Asynchronous comparator output drives CTRIPOUTH */
    /* Input high = B3 */
    AnalogSubsysRegs.CMPHPMXSEL.bit.CMP3HPMXSEL = 3;  /* 3 : B3 High Positive */
    /* Trip zone on EPwmA */
    EPwmXbarRegs.TRIP7MUX0TO15CFG.bit.MUX4 = 0;       /* Configure TRIP5 to be CTRIP3H */
    EPwmXbarRegs.TRIP7MUXENABLE.bit.MUX4 = 1;         /* 1: Respective output of Mux0 is enabled to drive the TRIP5 of EPWM-XBAR */
    /* Output to pin */
    OutputXbarRegs.OUTPUT5MUX0TO15CFG.bit.MUX4 = 0;   /* 00 : Select .0 input for Mux0 */
    OutputXbarRegs.OUTPUT5MUXENABLE.bit.MUX4 = 1;     /* 1: Respective output of Mux0 is enabled to drive the OUTPUT5 of OUTPUT-XBAR */
    //GpioDataRegs.GPASET.bit.GPIO28 = 0;
    GpioCtrlRegs.GPADIR.bit.GPIO28 = 1;               /* 1: The pin is an output */
    GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1;
    GpioCtrlRegs.GPAGMUX2.bit.GPIO28 = 1;
    EDIS;

  • Hi Francois,

    I'm glad you have found a workaround but the solution is a bit odd. I have never seen this. I wonder if it has something to do with the read-modify-write of PCLKCR14 since it contains clock turn-on for all the CMPSS. If you can, please try a few experiments below so we can figure out what's happening.

    1. If you go back to your original code without the delay, after you enable both CMPSS1 and CMPSS3, can you check the COMPDACE bit of both CMPSS to see if they were indeed set to 1?

    2. To confirm this is not a read-modify-write issue, when enabling the clocks for CMPSS1 and CMPSS3 using PCLKR14, instead of using CpuSysRegs.PCLKCR14.bit.CMPSS1 and CpuSysRegs.PCLKCR14.bit.CMPSS3, use CpuSysRegs.PCLKCR14.all. In CMPSS1 config code, write a value that only turns on CMPSS1. In the CMPSS3 code, write this to a value that turns on both CMPSS1 and CMPSS3.

  • Hi Frank,

    Further to your advice, I've test the following :

    1) 

    Remove my workaround

    When I initialized both CMPSS (1 then 3), 3 is not working

    PCLK14 = 0x0000 0005 (Both CMPSS are clocked)

     Cmpss1Regs.COMPCTL.COMPDACE = 1  -> OK

     Cmpss3Regs.COMPCTL.COMPDACE = 0  -> Bad (this is the problem)

    2)

    Remove my workaround

    Put CpuSysRegs.PCLKCR14.all = 0x0001; in Comp1Init()

    Put CpuSysRegs.PCLKCR14.all = 0x0005; in Comp3Init()

    PCLK14 = 0x0000 0005 (Both CMPSS are clocked)

    Cmpss1Regs.COMPCTL.COMPDACE = 1  -> OK

     Cmpss3Regs.COMPCTL.COMPDACE = 0  -> Bad

    I think the problem is a problem of stabilization of the clock, if I execute the program step by step with the debugger then it's OK.

    Best regards

    francois

  • Hi Francois,

    Thanks for performing the additional debug. Yes you are right, this is looking like a clock delay issue. This behavior is unexpected. Even if there was a clocking delay before the modules can be configured, i would expect both CMPSS1 and CMPSS3 to require the same delay but based on your analysis, CMPSS1 does not require a delay while CMPSS3 does.

    If you don't mind, can you ran one more experiment? I want to confirm which CMPSS exhibit this behavior. Can you repeat the same experiment for all 7 CMPSS? Turn on the clock for each CMPSS, write to COMPDACE and check if it was set to 1.

  • Hello Frank,

    I've done the Following and here here the results :

    EALLOW;
    CpuSysRegs.PCLKCR14.bit.CMPSS1 = 1;               /* 1: Module clock is turned-on. */
    Cmpss1Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS2 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss2Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1;               /* 1: Module clock is turned-on. */
    Cmpss3Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS4 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss4Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS5 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss5Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS6 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss6Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS7 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss7Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    EDIS;
    -> CMPSS3 non enabled (this confirm our original issue)
    EALLOW;
    CpuSysRegs.PCLKCR14.bit.CMPSS1 = 1;               /* 1: Module clock is turned-on. */
    Cmpss1Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS2 = 1;               /* 1: Module clock is turned-on. */
    Cmpss2Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1;               /* 1: Module clock is turned-on. */
    Cmpss3Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS4 = 1;               /* 1: Module clock is turned-on. */
    Cmpss4Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS5 = 1;               /* 1: Module clock is turned-on. */
    Cmpss5Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS6 = 1;               /* 1: Module clock is turned-on. */
    Cmpss6Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS7 = 1;               /* 1: Module clock is turned-on. */
    Cmpss7Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    EDIS;
    -> CMPSS7 non enabled
    EALLOW;
    CpuSysRegs.PCLKCR14.bit.CMPSS1 = 1;               /* 1: Module clock is turned-on. */
    Cmpss1Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS2 = 1;               /* 1: Module clock is turned-on. */
    Cmpss2Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1;               /* 1: Module clock is turned-on. */
    Cmpss3Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS4 = 1;               /* 1: Module clock is turned-on. */
    Cmpss4Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS5 = 1;               /* 1: Module clock is turned-on. */
    Cmpss5Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    CpuSysRegs.PCLKCR14.bit.CMPSS6 = 1;               /* 1: Module clock is turned-on. */
    Cmpss6Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    //CpuSysRegs.PCLKCR14.bit.CMPSS7 = 1;               /* 1: Module clock is turned-on. */
    //Cmpss7Regs.COMPCTL.bit.COMPDACE = 1;              /* 1 Comparator/DAC enabled */
    EDIS;
    -> CMPSS6 non enabled
    It sounds that the last comparator which is initialized is not done correctly.
    Best regards
    francois
  • Hi Francois,

    Thanks for the additional debug. This is interesting. Let me perform some local investigation and get back to you. Expect a reply by next week Tuesday.

  • Hi Francois,

    It turns out this issue has been identified locally and the affected devices already have updated documents reflecting this. This update was missed for the F28004x device. As you correctly identified, enabling the clocks to a module requires a delay before the module registers can be written. This delay is 5 NOPs. I have submitted a ticket to get this note added to the F28004x's TRM. Sorry about the inconvenience.

  • Hello Frank,

    Thanks for the confirmation for 5 nop, I'll implement your solution in all comparators initialization.

    Best regrads

    francois