Other Parts Discussed in Thread: TIDM-1007
Tool/software: Code Composer Studio
Dear Sir,
About the project of Design Guide: TIDM-1007, TIDU61B.
1) The first phase current IL1 is routed to CMPSS1, then from CMPSS1_CTRIPH_OR_L to route to XBAR_TRIP4, and then arrived to ePWM.
2) The second phase current IL2 is routed to CMPSS2, then from CMPSS2_CTRIPH_OR_L to route to XBAR_TRIP4, and then arrived to ePWM.
3) The third phase current IL3 is routed to CMPSS5, then from CMPSS5_CTRIPH_OR_L to route to XBAR_TRIP4, and then arrived to ePWM.
4) The total AC current is routed to CMPSS3, then from CMPSS3_CTRIPH_OR_L to XBAR_TRIP4, and then arrived to ePWM.
Because the XBAR_TRIP4 symbols are used to express in the program of pfc1ph3ilttpl_board.c, I cannot distinguish which ePWM is routed from IL1, IL2, IL3 and AC current for those currents with the same name by XBAR_TRIP4.
Namely, I want to know to which ePWM where IL1, IL2, IL3 and AC current are connected to.
I would very appreciate if anyone can resolve my questions and point out the line number and the routine’s name.
Best Regard
Hung-Jin Chen