This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Dual Code Security Module Differences with TMS320F28379

Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMS320F28379S,

Greetings,

We are currently using the TMS320F28379S and D, and are considering migrating some of our code, including the DCSM code, to the TMS320F280049C.  I have only been able to find a datasheet for the 280049C and the information on the DCSM is very high level.  But it exactly matches the text which is in the 28379's datasheet.  I have not been able to find a TRM for the 280049C to determine if the two DCSM modules are, in fact, the same, which would allow the re-use of the code we are using on the Delfino.  So two questions:

  1. Is the DCSM in the 280049C the same as the 28379?
  2. Is there a TRM for the TMS320F280049C?

Thank you,

Ed