Part Number: TMS320F28032
Hi
I am using EPWM1A of TMS320F28032 to control my single-ended inverter and I captured a false pulse during the operation.
The normal pulse width is about 5us and the false pulse width is about 53us.
I am using an up count for the counter. PWM output high when counter is zero and when counter equals to CMPA it will output low. The total PWM period is 66.7us(15kHz) but I am not using all the period time. I have a sync signal input to EPWM1 and when receive sync signal, counter will load phase shift value to finish the period earlier than 66.7us. Normal period is about 40us and pulse width is about 5us. The false pulse comes with width of 50us.
I found one note in the manual "NOTE: An EPWMxSYNCI external synchronization event can cause a discontinuity in the TBCTR count sequence. This can lead to a compare event being skipped. This skipping is considered normal operation and must be taken into account." I am suspecting it may be related to this but cannot confirm.
Can you please help to give some suggestion about my failure?
Below is my setting and control for EPWM1.
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; //TB_SYNC_DISABLE
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm1Regs.AQSFRC.bit.RLDCSF = CC_CTR_ZERO;
EPwm1Regs.TBPRD = PWM1_TIMER_TBPRD_10KHZ;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;//TB_COUNT_UP; // Count up
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;//;ET_CTR_PRD; // Select INT on Period event
EPwm1Regs.ETSEL.bit.INTEN = 0; // Disenable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event
EPwm1Regs.ETCLR.bit.INT = 1;
/* Generate PWM */
EPwm1Regs.CMPA.half.CMPA = (EPwm1Regs.TBPRD*3>>5);
EPwm1Regs.CMPB = (EPwm1Regs.TBPRD>>2);
EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE;
u32delay = ((EPwm1Regs.TBPRD>>3));
EPwm1Regs.TBPHS.half.TBPHS = 0;
EPwm1Regs.TBPHS.half.TBPHS = u32delay;
EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLB.bit.CAU = AQ_CLEAR;
EPwm1Regs.DBCTL.bit.HALFCYCLE = 0;
EPwm1Regs.DBCTL.bit.IN_MODE = DB_DISABLE;//DBA_RED_DBB_FED;
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_DISABLE;//DB_FULL_ENABLE;
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm1Regs.DBRED = 0;
EPwm1Regs.DBFED = 0;
/* for ADC trigger */
#if 1
EPwm1Regs.ETSEL.bit.SOCBEN = 1; // Enable SOC on B group
EPwm1Regs.ETSEL.bit.SOCBSEL = 6;//2; // Select SOC time-base counter equal to CMPB when the timer is incrementing
EPwm1Regs.ETPS.bit.SOCBCNT = 1; //1 event has occurred.
EPwm1Regs.ETPS.bit.SOCBPRD = 1; // Generate pulse on 1st event
#define SET_PWM_DUTY(X) {EPwm1Regs.TBPRD = GET_15K_PWM_PRD;\
EPwm1Regs.CMPA.half.CMPA = ((uint32)(Base_Time_10us * ((uint32)(X)) >>10));\
EPwm1Regs.CMPB = EPwm1Regs.CMPA.half.CMPA ; \
EPwm1Regs.TBPHS.half.TBPHS = ((uint32)(EPwm1Regs.TBPRD-(EPwm1Regs.TBPRD>>9) * Delay_Time));}