Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi E2E,
I am using TMS320F28379D. I am trying to configure interrupts for SCI in CPU1 and use SCI in CPU2. Could you please help me how to configure the interrupts?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi E2E,
I am using TMS320F28379D. I am trying to configure interrupts for SCI in CPU1 and use SCI in CPU2. Could you please help me how to configure the interrupts?
Thanks.
Hi,
Not sure why you want to setup interrupt on CPU1 when SCI is assigned to CPU2 but interrupt are triggered on both the CPU so you just need to enable SCI interrupt on CPU1 PIE and map the interrupt handler in vector table to have it working.
Please refer SCI example in C2000Ware to see how to setup the interrupts.
Regards,
Vivek Singh
Hi Vivek Singh,
Thank you so much for your reply. Actually, we would like to use SCI in CPU2 and want to know if we need assign SCI to CPU2 in CPU1.
We have assigned SCI to CPU2 in CPU1 with the following code and configure corresponding interrupts
EALLOW;
DevCfgRegs.CPUSEL5.bit.SCI_C = 1;
EDIS;
and configure corresponding interrupts in CPU2 with the following code:
EALLOW;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieVectTable.SCIC_RX_INT = &Receive;
PieVectTable.SCIC_TX_INT = &Send;
EDIS;
SCI still can no work.
If we want to use SCI in CPU2, we need to configure corresponding GPIOs in CPU1 then assign to CPU2 or directly in CPU2?
Thanks.
Hi,
If we want to use SCI in CPU2, we need to configure corresponding GPIOs in CPU1 then assign to CPU2 or directly in CPU2?
GPIO (PINMUX) configuration can be done by CPU1 only. So user need to configure the pinmux and then assign the SCI to CPU2. Please note that SCI clock need to be configure in CPU2 only.
Regards,
Vivek Singh