This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280041C: InstaSPIN compilation

Part Number: TMS320F280041C
Other Parts Discussed in Thread: C2000WARE,

Tool/software: Code Composer Studio

Greetings! I`m using the CCS and InstaSPIN lib for a very first time! So I`ve loaded a few examples from C2000Ware_MotorControl_SDK_2_01_00_00. In all example in Properties->General the option Variant is set to "Generic C28xx Device". Do I have to change it to my controller(TMS320F280041C) before release build? I`ve already tried that and I receive errors -> I think it`s something connected with the linker files. So after I tried to switch back to Generic C28xx Device -> again I received errors. How can I fix that or everytime I have to start all over. For now my projects are always based on an example project! 

Thanks!