This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35M22C: G3 FCC source code for F28M35 MCU & AFE032 combination

Part Number: F28M35M22C
Other Parts Discussed in Thread: AFE032

We have made a board with F28M35 MCU and AFE032 for PLC based data acquisition.

Due to some reasons, we couldn't start the firmware development. Now we are actively perusing that. 

Can we get the link for the G3 FCC source code for the F28M35 MCU & AFE032 combination?

We have asked this before but the link was not approved at that time..

  • Bibin,

    I'm looking into this, will try an have a response by the end of the day today.

    Best,

    Matthew

  • Bibin,

    Apologies for the delay, I'm still working on locating the appropriate files.

    I also want to take the opportunity to make sure there is clarity on what we can provide both in terms of packages and support.

    1)The packages that are available will be delivered for both the Service Node(SN) and Data Concentrator(DC)

    2)We provide both SDKs and DDKs, but not full source for these PLC packages.

    3)TI has stopped development/investment in this application as of 2017, as such the packages are consistent with G3 standard set forth in 2016

    4)Along with #3, TI is not able to provide development support either for FW or HW kits related for PLC modems from TI.  

    As soon as I get more clarity on the package location I will update the post, I appreciate your patience in this regard.

    Best,

    Matthew

  • Bibin,

    I have renewed/granted access to the requested packages.

    Best,
    Matthew