Part Number: TMS320F280049
Hi Experts,
Please refer to the attached file.
It is related the e2e thread https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/913822.
Let me clarify the units for each setting as follows.
(1) Md_A : 0 to 0xFFFF ( resolution TBCLK )
(2) Md_B : 0 to 0xFFFF ( resolution TBCLK )
(3) Delta phi: 0 to 360 degree, Is it possible to make like a delay?
(4) T1_a : 0 to 0x3FFF ( resolution TBCLK )
(5) T1_b : 0 to 0x3FFF ( resolution TBCLK )
(6) Tpwm : 0 to 0xFFFF (resolution TBCLK )
Am I making sense?
If HRPWM is utilized, (1), (2), and (6) can be set HR, however, (4) and (5) can not use HR mode.
Am I correct?
I would like to know the number of decimal places for HRPWM.
Thank you for your help.
Best regards,
Hitoshi20200630_F280049_ePWM_output_q53.pdf